Technical FAQs

Ask a Question

What are the acceptable wire sizes for the Class 8910 Type DP definite purpose contactors?

As listed below based on device used:

Class 8910 Type DP11, DP12, DP21, DP22, DP31, DP32 will accept 14 awg to 8 awg solid or stranded coper wire only.

Class 8910 Type DP41, DP42 will accept 14 awg to 6 awg solid or stranded coper wire only.



CTA-ID : 2015749
Was this helpful?
What can we do to improve the information ?