Technical FAQs

Ask a Question

Pilot Light Replacement for an 8539 NEMA 7/9 combination starter

Issue:
Are replacement pilot lights available for our Nema 7/9 8538/8539 combination starters?

Product Line:
Nema starters sold and supported in the USA.

Environment:
Maintenance

Cause:
Selection/replacement

Resolution:
The Nema 7/9 enclosures are no longer available for our Nema starters/contactors.  We have no explosion proof enclosures available for these, effective 2011. 

CTA-ID : 2016246
Was this helpful?
What can we do to improve the information ?