Technical FAQs

Ask a Question

Can I wire an XS type proximity sensor to directly control a Size 3 contactor?

No. The XS prox sensor is only capable of handling 200ma output current. The Size 3 contactor coil requires much more. Recommend using an interposing relay to switch the contactor coil.

CTA-ID : 2016443
Was this helpful?
What can we do to improve the information ?