Technical FAQs

Ask a Question

Why is a Square D starter with an H108, H208, H118, or H218 suffix not a good number?

The ``8`` special overload contactor size combination is only offered with Feature Unit solid state overload relays. Therefore the ``H`` code would have to be H308 or H318.

CTA-ID : 2016440
Was this helpful?
What can we do to improve the information ?