Technical FAQs

Ask a Question

What is the consumption of the control coil for Class 8502 or 8536 Type SC contactor / starter?

Issue:     
Identifying coil consumption of a NEMA size 1 contactor or starter

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Identifying coil consumption 

Resolution:
245 VA inrush and 27 VA sealed for 60 hertz or 232 VA inrush and 26 VA sealed for 50 hertz.

This also applies to all 8538SC, 8539SC, 8606SC, 8630SC, 8640SC, 8702SC, 8736SC, 8738SC, 8739SC, 8810SC, 8903SM, 8940 Size 1 except ``NP``, 8941NC, 8941CC, 8941UC, and 8941DC devices.


 
Was this helpful?
What can we do to improve the information ?