Technical FAQs

Ask a Question

Are the IEC K-Line contactors SEMI F47 compliant?

Product Line:

Tesys K Line Contactors
 
Resolution:
K-Line contactors are SEMI F47 compliant. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.

The K-Line offering is available in 6 amp and 9 amp versions for SEMI F47 when used with 24 and 120 volt ac control coils. All DC controlled versions are SEMI F47 compliant as standard.

All K-Line products carry the UL, IEC and CE markings. For additional information and other products for SEMA F47 applications refer to the attached link.



CTA-ID : 2017163
Was this helpful?
What can we do to improve the information ?