Technical FAQs

Ask a Question

Are the IEC F-Line contactors SEMI F47 compliant?

Product Line:
Tesys F Line Contactors and Accessories

F-Line contactors are SEMI F47 compliant and perfect for EMO contactor applications. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.

The F-Line offering is available from 115 to 780 amp versions.

F-Line contactors are designed to accept ring terminals for wire terminations and all carry the UL, IEC, and CE markings. For additional information and other products for SEMA F47 applications refer to the attached link.

CTA-ID : 2017161
Was this helpful?
What can we do to improve the information ?