Technical FAQs

Ask a Question

Does the Square D Nema 3R heavy duty safety switches have side hinged covers/doors?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Cover design

Cause:
Application

Resolution:
ALL the NEMA 3R, current Series F up to 200amp and ALL the NEMA 3R, current Series E 600amp through 1200amp Heavy Duty Safety Switches have Side Hinged covers/doors.

NOTE: ALL NEMA 12/3R Heavy Duty Safety Switches have a side hinged cover/door and can be used for NEMA 3R Applications. 



CTA-ID : 2017215
Was this helpful?
What can we do to improve the information ?