Technical FAQs

Ask a Question

Are replacement parts and auxiliary accessories still available for the Class 8508 pre-type S contactors?

Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** & **** represent ending digets depending upon voltage required.

All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.

If complete replacement device is required or desired, please use the Competitive Cross Reference tool link below.


CTA-ID : 2017069
Was this helpful?
What can we do to improve the information ?