Technical FAQs

Ask a Question

What is the inrush and sealed VA for an LC1F265 contactor coil ?

Product Line:
 
Tesys F line Contactors and Accessories
 
Resolution:
 
40 - 400 Hz coil - 650 VA Inrush, 10 VA sealed @ 50 or 60 Hz.






CTA-ID : 2016956
Was this helpful?
What can we do to improve the information ?