Technical FAQs

Ask a Question

Can a power pole be added to an 8903 Type S 60A lighting contactor?

Yes, order a 9999 SB21 for one normally open; 9999 SB22 for one normally closed; 9999 SB23 for one normally open and one normally closed; 9999 SB24 for two normally open; 9999 SB25 for two normally closed.

Note: The total power contacts cannot exceed 5 poles.


CTA-ID : 2006122
Was this helpful?
What can we do to improve the information ?