Technical FAQs

Ask a Question

Are replacement parts and auxiliary accessories still available for the Class 8901 and Class 8903 lighting contactors?

Issue:     
Are replacement parts and auxiliary accessories still available for the Class 8901 and Class 8903 lighting contactors?

Product Line:
8901 and 8903 lighting contactors

Environment:
Products sold and used in the United States

Cause:
Replacement parts needed for 8901 and 8903 lighting contactors

Resolution:
Class 9999 Type R6 & R7 disconnect switch and circuit breaker electrical interlocks are still available.

Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** & **** represent ending digits depending upon voltage required.

All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.

If complete replacement device is required or desired, please use the Competitive Cross Reference tool.
Was this helpful?
What can we do to improve the information ?