Technical FAQs

Ask a Question

Is an FA100A rated NEMA Type 3R for outdoor use?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Clarification of NEMA ratings

Resolution:
No, the FA100A is rated NEMA 12K for indoor, dusttight application. It is not rated for outdoor use. For a NEMA Type 3R application consider either FA100RB or FA100AWK.


CTA-ID : 2017101
Was this helpful?
What can we do to improve the information ?