Technical FAQs

Ask a Question

What is the material content of the power contacts on the Class 8910 definite purpose contactors?

Consist of 85% silver and 15% cadmium oxide.


CTA-ID : 2017961
Was this helpful?
What can we do to improve the information ?