Technical FAQs

Ask a Question

Do NF panels use plug on or bolt on breakers?

Issue:
Do NF panelboards take bolt on or plug on breakers as standard?

Product Line:
NF panelboards sold and supported in the USA.

Environment:
Product features

Cause:
Are NF branch breakers considered bolt on or plug on?

Resolution:
The EDB, EGB, EJB breakers are bolt-on.



Revised 5/11/04


CTA-ID : 2017799
Was this helpful?
What can we do to improve the information ?