Technical FAQs

Ask a Question

What is the part number for the side joint covers (tie channels) for AP506G10?

Issue:
Side covers for bus duct / busway

Product Line:
Busway

Environment:
I-Line 

Cause:
Installation

Resolution:
The tie channel is 45202-026-01 and the screw bag assembly to attach it is 45132-001-55.
When ordering replacement tie channels, 2 tie channels and 2 bag assemblies are required per busway joint.
Was this helpful?
What can we do to improve the information ?