Technical FAQs

Ask a Question

What is the significance of the the little ``H`` on the front of the LRD TeSys overload relays ?

Issue: 
Identifying the H and A toggle switch on the front of a D line overload relay
 
Product Line:
Tesys D oveload relays
 
Environment:
Products sold and used in the United States
 
Cause:
There is a toggle on the front of the overload that says H on one side and A on the other.

 
 
Resolution:
The H stands for Hand. When the OLR`s are shipped from the factory, they are in the Hand Reset mode. Remove and discard this H ``cover`` and the OLR will be converted to Automatic Reset mode.


CTA-ID : 2018094
Was this helpful?
What can we do to improve the information ?