Technical FAQs

Ask a Question

Does Square D offer a shunt tripped breaker for use in the Q-Frame circuit breaker enclosures, for example the Q23225NRB?

Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures and Molded Case Circuit Breakers

Environment
Electrical Accessory

Cause:
Application

Resolution:
No. The Q-Frame enclosures ONLY accept the QBL, QDL, QGL, and QJL type breakers. These Q-Frame breakers do NOT accept any accessories such as shunt trips.


CTA-ID : 2018890
Was this helpful?
What can we do to improve the information ?