Technical FAQs

Ask a Question

Can QO-GFI and HOM-GFI breakers be tested using other manufacturers `GFI Testers` ?

Product Line:
QO-GFI Circuit Breakers
HOM-GFI Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
There may be some GFI testers on the market that work. However, it is recommended that the Push-to-test button on the breaker be used for testing and/or follow the steps in the instruction bulletin that come with the breakers.
 
Was this helpful?
What can we do to improve the information ?