Technical FAQs

Ask a Question

How do I order a size 3 Class 8536 starter with a Motor Logic solid state overload relay that has a lower current range than the standard 30 - 90 amp size 3?

This is not an available option. The only Motor Logic SSOLR we have available for the size 3 starter is the one that has a current range of 30 - 90 amps.


CTA-ID : 2018257
Was this helpful?
What can we do to improve the information ?