Technical FAQs

Ask a Question

What is the difference between a 802103-026-50 12 circuit ground bar rated 225A and a 80103-026-51, with the same ratings.

Issue:
What is the difference between a 802103-026-50 12 circuit ground bar rated 225A and a 80103-026-51, with the same ratings.

Product Line:
Ground bar accessories for panelboards and load centers.

Environment:
Product Characteristics

Cause:
Selection

Resolution:
The 80103-026-51 ground bar used to have 25 holes and 23 terminations. When the 80103-026-50 became obsolete, the new 80103-026-51, was cut down to exactly the same circuit size (14 holes 12 terminations) , as the old 80103-026-50 bar.


8/31/04


CTA-ID : 2019677
Was this helpful?
What can we do to improve the information ?