Technical FAQs

Ask a Question

Are the QO and HOM load centers and branch breakers UL Series Short Circuit Current Rated and are the Load centers Marked?

Issue:
Product Features

Product line:
QO and Homeline load centers and branch breakers

Environment:
Short Circuit Current Rating(SCCR)

Cause:
Application

Resolution:
Yes, the QO and Homeline load centers do have UL Series Short Circuit Current Ratings.
The 2-Tier SCCR is located on the Box label inside the load center enclosure and the 3-tier SCCR label is located on the load center cover, These labels will show all the appropriate 2-Tier and 3-Tier UL listed Series Short Circuit Current Ratings(SCCR) for either an integral or remote(upstream) protection with the load center branch breakers. Also, attached is a pdf data bulletin for the load center Short Circuit Current Ratings.


 
Was this helpful?
What can we do to improve the information ?