Technical FAQs

Ask a Question

Is the FA breaker HACR rated?

Issue:
Is the FA breaker HACR rated?

Product Line:
FA/L Molded Case Circuit Breakers

Environment:
All FA/L Molded Case Circuit Breakers

Cause:
Need to use the FA/L breaker with group mount motors.

Resolution:
All UL Listed Molded Case Circuit Breakers are HACR type. Therefore all FA/L 15-100 amp breakers are HACR rated.


CTA-ID : 2020109
Was this helpful?
What can we do to improve the information ?