Technical FAQs

Ask a Question

Will the 14886 and 14887 ``end caps`` fit on the MG10285, MG10286, or the MG10287 comb bus?

No. The UL Recognized MG10285, MG10286, and the MG10287 comb bus is already insulated on the ends, and is NOT designed to be cut.
End cap MG14887 is designed to attach to the IEC rated comb bus.


CTA-ID : 2020219
Was this helpful?
What can we do to improve the information ?