Technical FAQs

Ask a Question

Do we make an 8903 PB contactor with a V02 voltage code for a 120Vac coil? How about for a 208V coil?

Yes, as of 7/30/2004, we now offer a 120VAC coil, which is ordered using voltage code V02 as shown in Digest 173 page 14-73, and for a 208V coil use V08. Voltage code V38 for a 120/208V coil is now invalid.

CTA-ID : 2019801
Was this helpful?
What can we do to improve the information ?