Technical FAQs

Ask a Question

On a UFP222RGFI, does removing the pullout disconnect both the power circuit and the GFCI receptacle circuit?

The UFP222RGFI pullout disconnects the 240Vac power circuit only. It does not control the 120Vac GFCI receptacle circuit. The GFCI receptacle should be controlled by the circuit breaker feeding the GFCI receptacle circuit.


CTA-ID : 2020275
Was this helpful?
What can we do to improve the information ?