Technical FAQs

Ask a Question

Can NEMA 1 MHC ``Door-In-Door`` trims be provided for ``trim to fit existing`` applications?

Issue:
Exterior NQOD trims

Product Line:
Panelboards

Environment:
NQOD

Cause:
Special trims

Resolution:
MHC Door-In-Door trims cannot be supplied for existing boxes unless the existing box is a Square D MH type and the correct size for the interior that is to be installed into it.


CTA-ID : 2021059
Was this helpful?
What can we do to improve the information ?