Technical FAQs

Ask a Question

Can the 9001K joystick operators be bought without contacts?<br /><br />

Product Line:

9001 type K 30 mm push button operators
 
Resolution:
 
Yes by dropping the H number on the end of the catalog number. Example 9001K35H2 is complete with contacts. Operator only is 9001K35.


CTA-ID : 2021067
Was this helpful?
What can we do to improve the information ?