Technical FAQs

Ask a Question

Do Enclosed ATS48 NEMA 3R have a cabinet heater installed as standard feature?

Per Development Engineering and Seneca, the standard 3R configuration does not include an enclosure space heater for the Enclosed 48 devices.
The ambient temperature range for 3R devices is 0 to 50 degrees C (32 to 122 degrees F).
If a heater is needed, go to the OE Tag Adder window and use (T232) as the Tag #


CTA-ID : 2021093
Was this helpful?
What can we do to improve the information ?