Technical FAQs

Ask a Question

What is the magnetic trip setting for a KA/KH breakers?

Product Line:
Legacy Circuit Breakers
KA Frame

Environment:
Electrical Distribution Equipment

Resolution:
The magnetic trip setting for the KA breakers below:

3 Pole (3P) Devices:

KA(L)36070 is 350 low, 700 High
KA(L)36080 is  400 low, 800 High
KA(L)36090 is 450 low, 900 High
KA(L)36100 is 500 low, 1000 High
KA(L)36110 is 550 low, 1100 High
KA(L)36125 is 625 low, 1250 High
KA(L)36150 is 750 low, 1500 High
KA(L)36175 is 875 low, 1750 High
KA(L)36200 is 1000 low, 2000 High
KA(L)36225 is 1125 low, 2250 High
KA(L)36250 is 1250 low, 2500 High

2 Pole (2P) Devices:

KA(L)26070 is 350 low, 700 High
KA(L)26080 is  400 low, 800 High
KA(L)26090 is 450 low, 900 High
KA(L)26100 is 500 low, 1000 High
KA(L)26110 is 550 low, 1100 High
KA(L)26125 is 625 low, 1250 High
KA(L)26150 is 750 low, 1500 High
KA(L)26175 is 875 low, 1750 High
KA(L)26200 is 1000 low, 2000 High
KA(L)26225 is 1125 low, 2250 High
KA(L)26250 is 1250 low, 2500 High

3 Pole (3P) Devices:

KH(L)36070 is 350 low, 700 High
KH(L)36080 is  400 low, 800 High
KH(L)36090 is 450 low, 900 High
KH(L)36100 is 500 low, 1000 High
KH(L)36110 is 550 low, 1100 High
KH(L)36125 is 625 low, 1250 High
KH(L)36150 is 750 low, 1500 High
KH(L)36175 is 875 low, 1750 High
KH(L)36200 is 1000 low, 2000 High
KH(L)36225 is 1125 low, 2250 High
KH(L)36250 is 1250 low, 2500 High

2 Pole (2P) Devices:

KH(L)26070 is 350 low, 700 High
KH(L)26080 is  400 low, 800 High
KH(L)26090 is 450 low, 900 High
KH(L)26100 is 500 low, 1000 High
KH(L)26110 is 550 low, 1100 High
KH(L)26125 is 625 low, 1250 High
KH(L)26150 is 750 low, 1500 High
KH(L)26175 is 875 low, 1750 High
KH(L)26200 is 1000 low, 2000 High
KH(L)26225 is 1125 low, 2250 High
KH(L)26250 is 1250 low, 2500 High

CTA-ID : 2020629
Was this helpful?
What can we do to improve the information ?