Technical FAQs

Ask a Question

What is the difference between a catalog number UFS222R and a UFP222R Air Conditioning Disconnect?

Issue:
Product selection

Product Line:
Air Conditioner Disconnect

Environment:
AC Disconnect

Cause:
Clarification

Resolution:
Both of these Air Conditioner Disconnects are obsolete and no longer available. The UFS222R preceeded the UFP222R and was purchased from Cutler-Hammer and brand labeled by Square D Company. The UFP222R replaced and was electrically equivalent to the UFS222R, however was manufactured by Square D Company. The QO200TR or QO200TRNM enclosed molded case switch is still offered by Square D/Schneider Electric for a 60A maximum, 240V air conditioner disconnect. The QO200TR is provided in a metallic enclosure, while the QO200TRNM is provided in a non-metallic enclosure.


CTA-ID : 2020456
Was this helpful?
What can we do to improve the information ?