Technical FAQs

Ask a Question

Can a FAL36060G breaker with a GFM100FA ground fault module be used in the FA100 F or S type circuit breaker enclosures?

Issue:
Product design

Product Line:
Circuit breaker enclosures

Environment:
breaker with ground fault module

Cause:
Application

Resolution:
No. The GFM module mounts to one end of the breaker and causes the length of both together, to be too long for the enclosure. So the FA100F or S type enclosures are too short. They could be used in the OLD KA225F or S enclosure types, BUT the KA enclosure are obsolete, No longer available with no direct replacement. Square D does not actually offer an enclosure anymore for use with both the FA breaker and GFM module.


CTA-ID : 2021514
Was this helpful?
What can we do to improve the information ?