Technical FAQs

Ask a Question

What external voltage kits are available for the Powerpact P and R frame breakers?

Issue:
What are the external voltage kits (EVS) for Powerpact P and R frame breakers?

Product Line:
Powerpact P and R

Environment:
Electrical Distribution Systems

Cause:
These kits sometimes need to be installed

Resolution:
NOTE: For Powerpact R and for Powerpact P frame (except motor operated), the EVS can be installed only in a breaker with an original trip unit type Ammeter and below (2.0, 3.0, 3.0A, 5.0, 5.0A, 6.0A).  It can not be installed in a Powerpact breaker if the original trip unit was a Power or Harmonic type.  These already have internal voltage sensing, and if it has internal voltage sensing, the ESV kit cannot be used.

Part numbers for field installable external voltage sensing kits are as follows:
S64203 EVS kit P frame unit mount / I-LINE
S64208 EVS kit R frame unit mount / I-LINE
S64209 EVS kit P frame drawout
S64210 EVS kit P frame motor operated / rotary handle


CTA-ID : 2021708
Was this helpful?
What can we do to improve the information ?