Technical FAQs

Ask a Question

What is the catalog number for the test module needed to test Micrologic type ME, MX, NE, NX, PE, PX and SE, Series 5 and 5A breakers?

Issue:
What is the catalog number for the test module needed to test Micrologic type ME, MX, NE, NX, PE, PX and SE, Series 5A breakers?

Product Line:

Environment:

Micrologic trip unit series 3 and A.  (not to be confused with breaker series number on the breaker).

Cause:

Resolution:
CBTM4A is the test module needed to these Series 3 and A trip units.


CTA-ID : 2021626
Was this helpful?
What can we do to improve the information ?