Technical FAQs

Ask a Question

What is the inrush/current draw of the shunt trip coil MG26974? It is a 24VAC shunt trip for a C60N Merlin Gerin breaker.

Product Line:
Circuit Breakers
M9

Environment:
Electrical Distribution Equipment

Resolution:
That unit has a momentary draw of 120 W.


CTA-ID : 2021896
Was this helpful?
What can we do to improve the information ?