Technical FAQs

Ask a Question

How many and what size conductor(s) will the lug accept on the Class 8903 Type SX* lighting contactor?<br /><br />* = A, C, F, G, H, O, W, followed by 1 or 2 digits; i.e. 8903SXG1, 8903SXA70.

Control - Two 16 AWG to 12 AWG copper conductors per terminal.

Power - (1) 4 AWG to 600 MCM copper or aluminum conductor per phase or (2) 0 AWG to 250 MCM copper or aluminum conductors per phase.


CTA-ID : 2022378
Was this helpful?
What can we do to improve the information ?