Technical FAQs

Ask a Question

What type of circuit breakers are installed in the Night Master enclosed lighting contactors?

30 amp is FAL36030, 60 amp is FAL36060, 100 amp is FAL36100, and the 200 amp is KAL36200.


CTA-ID : 2022556
Was this helpful?
What can we do to improve the information ?