Technical FAQs

Ask a Question

Are factory modifications Forms G10 or G101 available on Class 8903 Lighting contactors in NEMA 4/4X enclosures?

No, the receptacles and photo cells do not have NEMA 4/4X ratings are therefore cannot be supplied in this enclosure.


CTA-ID : 2022300
Was this helpful?
What can we do to improve the information ?