Technical FAQs

Ask a Question

What is the field installable padlock attachment for the Masterpact NW W/Y frame breaker, or NT?

Issue:
What is the field installable padlock attachment for the Masterpact NW W/Y frame breaker, or NT?

Product Line:
Masterpact

Environment:
Products sold in North America

Cause:
Need to padlock open an existing Masterpact NW or NT

Resolution:
S48539 for Masterpact NW,  W and Y frame. S47514 for the Masterpact NT

Padlock attachment S48539

See instruction bulletin, 48049-197-02


See instruction bulletin, 48049-233-01



CTA-ID : 2022721
Was this helpful?
What can we do to improve the information ?