Technical FAQs

Ask a Question

Is there a 12VDC shunt trip available for the LA / LAL / LH / LHL / Q4 breaker?

Issue:  
There is not a 12VDC suffix code in the supplemental digest.  

Product line: 
Molded case circuit breakers 

Environment:  
LA LAL LH LHL Q4 Q4L circuit breakers Series 4 or newer

Resolution:  
Yes but ONLY if the breaker is series 4 or newer.  Use suffix 1039 for factory-installed, or LA11039 for a field-installable kit.  
Was this helpful?
What can we do to improve the information ?