Technical FAQs

Ask a Question

What is the suffix -1680 on the PAF361600DC-1680 breaker?

Issue:  
What does the 1680 suffix indicate on a PAF frame breaker?  

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
It is a 48V dc undervoltage release (suffix 1128), two normally open and two normally closed auxiliary contacts gold flashed (suffix 1286), special 48`` leads, and UL approved.
Was this helpful?
What can we do to improve the information ?