Technical FAQs

Ask a Question

How can I replace or get parts for a Masterpact MP, M, or MC breaker?

Issue:
How to get a replacement for an old-style Masterpact breaker

Product Line:
Masterpact MP

Environment:
Electrical Distribution Systems and OEM

Cause:
Breakers need to be replaced

Resolution:
Masterpact MC and M (ANSI and IEC rated) breakers are not available.
A limited offering of Masterpact MP (UL Listed) breakers are available.  First determine:
  • Fixed or Drawout construction
  • The breaker amperage
  • Whether it has ground fault protection or not (LSI or LSIG)
The following catalog numbers are available as of October 2014:
Amps       Fixed 3p        Drawout 3p
1600 A     MP100135     MP100136      
2000 A     MP100137     MP100138      
3000 A     MP100139     MP100140      

Only a limited number of accessories are still available.  Check Supplemental Digest for availabilitly. 
If replacement breaker is not available, it may be necessary to upgrade to the Masterpact NW.  Contact Schneider Services or sales office for assistance.
Was this helpful?
What can we do to improve the information ?