Technical FAQs

Ask a Question

What is the LA34400MC circuit breaker?

Product Line:
Legacy Circuit Breakers

Electrical Distribution Equipment

It is a 480V rated thermal-very high magnetic withstand circuit breaker for Mission Critical Loads. The magnetic setting is factory preset at 20 X thermal rating.

CTA-ID : 2022953
Was this helpful?
What can we do to improve the information ?