Technical FAQs

Ask a Question

What is the catalog number for replacement mechanical lugs for HD, HG, HJ, HL circuit breakers?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Catalog number is AL150HD which is a set of 3 lugs with a wire range of 1 -#14 to 3/0 AWG AL or CU .


CTA-ID : 2023083
Was this helpful?
What can we do to improve the information ?