Technical FAQs

Ask a Question

Is the OEM mounting base QON816L100, UL Listed or CSA Certified?

Issue:
Standards

Product Line:
OEM Mounting Base

Environment:
OEM Mounting Base

Cause:
Clarification of standards met

Resolution:
The QON816L100 OEM Mounting Base is listed as a UL Recognized Component (File E6294) and a CSA Panelboard Interior (File LL89066). The final acceptance of his component is dependant upon its installation and use in complete equipment submitted to UL or CSA by the OEM. UL


CTA-ID : 2023246
Was this helpful?
What can we do to improve the information ?