Technical FAQs

Ask a Question

Are Gold contacts available on the Class 8910 Type DPA contactors?

Power contacts are not available as gold. However, the 9999D auxiliary contacts are available with gold flashed contacts. Add form Y237. For example, 9999D10Y237. Please note this only applies to 8910 Type DPA12 through DPA 93 contactors. Gold flash auxiliary contacts are not available for the 8910 Type DPA 123 Type 123 or Type SYD.

CTA-ID : 2023129
Was this helpful?
What can we do to improve the information ?