Technical FAQs

Ask a Question

Is replacement 24 volt control coil still available for Class 8536 Type A (Pre-Type S) starter?

Yes, 31012-400-23 is the replacement 24 vac 60 hertz control coil for Series B & C NEMA size 00 contactor / starter only.

CTA-ID : 2022806
Was this helpful?
What can we do to improve the information ?