Technical FAQs

Ask a Question

What is the difference is between a EHB breaker and a EDB breaker?

Issue:
Can an EDB breaker replace an EHB breaker?

Product Line:
EDB Breakers

Environment:
This applies to all EHB and EDB, EGB, EJB breakers

Cause:
Can the EHB breaker be installed in an NF panel or the EDB be installed in the EHB panel?

Resolution:
The EHB is used in NEHB panels and the EDB is used in NF panels.
The EHB breaker is 1" wide by 4.03" long and the EDB breaker is 1" wide and 5.625" long.
The EHB breaker is obsolete with no replacement.  
Was this helpful?
What can we do to improve the information ?