Technical FAQs

Ask a Question

What material is the XVBC02 & XVBC11 made of?

Issue:
What material is the XVBC02 & XVBC11 made of?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
The XVBC02 is stainless steel (matte black finish). The XVBC11 tulip is a Zinc alloy (black matte finish).


CTA-ID : 2023180
Was this helpful?
What can we do to improve the information ?