Technical FAQs

Ask a Question

Will a LAD4RCE or LA4DRCU also fit a LC2D09 thru LC2D38 reversing contactors?

Issue:
Identifying accessories for reversing contactors

Product Line:
IEC contactors and starters

Environment:
Products sold and used in the United States

Cause:
Accessories used on non-reversing contactors are also needed for reversing application

Resolution:
Yes, the LC2D contactors are provided standard with one on the left contactor. One may be added to the right contactor.


CTA-ID : 2022733
Was this helpful?
What can we do to improve the information ?